Did you know as of 2017, the NEC requires that kitchen and laundry areas have both arc fault and ground fault protection. Eaton’s AF/GF receptacles provide protection from both arc and ground faults using Eaton’s 15 years of arc fault experience. In addition, the AF/GF receptacles are equipped with self-test GFCI technology to ensure the proper operation of the protection circuitry. These receptacles also add the convenience of a local reset, best for applications where the breaker panel is difficult or inconvenient to access.
Copyright Eaton 2021 · All rights reserved